2022-03-28 03:13 AM
Hi,
currently I can't open any .ioc file which hasn't been previously created with my computer.
There's no problem if I open an .ioc file inside CubeIDE, but, when I want to use VS Code I need to open the .ioc file using just CubeMX.
If I open an .ioc file with CubeMX, the program brings me the startup page. Whether I try to load a project directly from CubeMX, I can't navigate through the folders because, even in the Desktop folder the file navigator shows me an empty space.
Does anyone have my same problem, with MacOS?
Solved! Go to Solution.
2022-03-28 03:22 AM
Hi @f4_kiddo,
Can you follow the solution described in this post ?
STM32CubeMX 6.4.0 doesn't interact nicely with MacOS 12.1 (Monterey)
Let me know the result.
Regards,
Aymen.
2022-03-28 03:22 AM
Hi @f4_kiddo,
Can you follow the solution described in this post ?
STM32CubeMX 6.4.0 doesn't interact nicely with MacOS 12.1 (Monterey)
Let me know the result.
Regards,
Aymen.
2022-03-28 04:15 AM
Thank you so much!
Now it's working fine
2022-07-17 04:36 AM
I was having the same problem and this solution worked for me. Thank you.
Although I will say that this shouldn't be an issue that we should be struggling with. I don't remember this being an issue when I installed an earlier version of CubeMX.
2022-07-17 04:44 AM
Intended a reply on my initial comment
"I was having the same problem and this solution worked for me. Thank you.
Although I will say that this shouldn't be an issue that we should be struggling with. I don't remember this being an issue when I installed an earlier version of CubeMX."