cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-NFC3 not installing through STM32CubeMX

Geminus_Leonem
Associate II

When trying to install X-CUBE-NFC3 from https://www.st.com/en/embedded-software/x-cube-nfc3.html through  STM32CubeMX I get the following error message: 

image.png

There most likely are files missing from the X-CUBE-NFC3 zip provided: 

Geminus_Leonem_0-1716830066727.png

 

Any help on the matter would be appreciated.

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @Geminus_Leonem and welcome to the ST Community 😊.

Some CUBE packages were made available before the introduction of the free GUI STM32CubeIDE and could not be installed in STM32CubeMX at that time. However, it was already quite easy to integrate the file structure of the CUBE package into one's own project. You could refer to this FAQ on How to add external libraries in STM32CubeIDE - STMicroelectronics Community.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for the reply.

Unfortunately, the linked FAQ does not help with the issue at hand as it doesn't explain how to implement the Middleware files through the IDE.

Any help to someone new to ST regarding this issue would be greatly appreciated.