cancel
Showing results for 
Search instead for 
Did you mean: 

Why the use of ST's Middlewares is soo haaaaard? STM32WLE5 CMSIS DSP LoRa

lemke.a.w
Associate III

I'm trying to use the DSP Library on the STM32WLE5CCU6 and some error messages appear on STM32CubeIDE. I have the same code tested and running on STM32F103C8T6 and STM32F407VET6 without any problem.

lemkeaw_0-1714512816698.png

STM32CubeIDE Version: 1.14.0 Build: 19471_20231121_1200 (UTC)

STM32CubeMX Version 6.10.0

STM32CubeWL Firmware Package v1.3.0 / 09-November-2022

STMicroelectronics.X-CUBE-ALGOBUILD DSP Library Library 1.3.0

I'm seriously thinking about switching to using any other STM32 with an external SX1262 chip via SPI interface than the STM32WL with its related libraries. The LoRa middleware is impossible to work with, I am forced to provide an UART interface  (Why not use SWV / ITM interface ?) and the ADC , I cannot disable it.

This kind of thing sometimes makes me think about giving up on ST!

 

 

 

 

 

 

 

 

12 REPLIES 12

Could it be related to the STM32WLE5 not having FPU?

Yes Indeed. Glad to know that the problem is fixed.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

BarryWhit
Lead II

*correction*

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.

Done, thank you @BarryWhit .

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.