cancel
Showing results for 
Search instead for 
Did you mean: 

Why is the core_cm4.h file not generated then?(stm32L476RG)

Essayator
Associate III

Hello,

I am beginner with stm32, I try to start my first project but I cannot do it, because there is the core_cm4.h file which was not generated here is the error message: Description Resource Path Location Type

fatal error: core_cm4.h: No such file or directory stm32l476xx.h /bliking-test/Drivers/CMSIS/Device/ST/STM32L4xx/Include line 165 C/C++ Problem

10 REPLIES 10
KnarfB
Principal III

What tools are you using to generate the code, what tool versions, what OS?

Normally, it *is* generated.

hth

KnarfB

Essayator
Associate III

I found the file I copied it to the folder, there my code works but I can't read data from a sensor (pmodgyro)

Sara BEN HADJ YAHYA
ST Employee

Hello @Essayator​ ,

Could you please share your ioc file or provide us with the scenario that led to this issue?

Thanks,

Sara.

Hello @Sara BEN HADJ YAHYA​ ,

can I share my file ioc in the comment if not how to share it

Hello @Essayator​ ,

Yes you can attach the ioc in a comment.

Sara.

Essayator
Associate III

here is my file

 

I have another other problem when I run the code in ide, the ide sends me to assembler code that I don't understand but seems to be a reset

Hello @Essayator​ ,

There is no issue when I generated a project using your ioc. I even created a new project from scratch and I didn't face any error during the build.

Please copy your ioc file in a new folder and generate a new project.

I hope this helps :)

Sara.