2021-01-04 4:36 PM
I made a project based on NECLEO STM32L552ZE-Q, when I made it from MX configuration tool, I found there was no "stm32l5xx_hal.h", while it was included in main.c, where could I find it?
2021-01-20 12:40 AM
The recent time, I ran the code, it didn't show the error, and the code has been updated into board, since when I push the user button, I saw the first time what I expected, but I couldn't communicate with it by serial port, I guesses maybe as you said " the HAL_UART_MODULE_ENABLED and HAL_USART_MODULE_ENABLED" has not been enabled. But I could not fine the file"stm32l5xx_hal_conf.h", although I could find file "stm32l5xx_hal.h" there.
And, the board was shown as "STMicroelectronics STLink Virture COM Port (COM7)" in"Devices Manager" of Windows 10, I could only find COM1(Communications Port) in Putty.
2021-01-20 12:51 AM
OK, I found it, it was here:
/...(project name)/Core/Inc/stm32l5xx_hal_conf.h
2021-01-20 1:30 AM
I just tested in VS Code, it was said COM7 connected, no problem no error, but I just could input into it, and could see output from board in it.
2021-01-20 7:08 AM
> But I could not fine the file"stm32l5xx_hal_conf.h", although I could find file "stm32l5xx_hal.h" there.
It's shown in the screenshot in your very top post. You're going to need to try a little harder here if you want to solve issues.
2021-01-20 5:44 PM
“HAL_UART_MODULE_ENABLED�? was found in NonSecure's "stm32l5xx_hal_conf.h" after MX. Since I have set LPUART1 as "asynchronous" , so USART is not needed.