2023-04-17 12:12 AM - edited 2023-11-20 7:58 AM
STM32F407 Discovery
en.MB997-F407VGT6-C01_Schematic.pdf
HSE quartz 8 megahertz.
How are 4-26 MHz generated for HSE?
With an oscilloscope, I see only 8 megahertz on X2 quartz.
Where are those 25 megahertz that are listed as input for HSE?
In the documentation I read this:
This frequency cannot be changed, it is fixed at 8 MHz and connected to PH0-OSC_IN of the STM32F407VG.
But in Cube Mx this frequency can be changed from 4 to 26 megahertz.
Solved! Go to Solution.
2023-04-17 12:35 AM
>Where are those 25 megahertz that are listed as input for HSE?
on a board with 25MHz crystal (i have one of these here)
> in Cube Mx this frequency can be changed from 4 to 26 megahertz
how should Cube know, what crystal you decide to use ???
>it is fixed at 8 MHz and connected to PH0-OSC_IN
exactly. until you solder another crystal there in. then set this new frequency in Cube!
2023-04-17 12:35 AM
>Where are those 25 megahertz that are listed as input for HSE?
on a board with 25MHz crystal (i have one of these here)
> in Cube Mx this frequency can be changed from 4 to 26 megahertz
how should Cube know, what crystal you decide to use ???
>it is fixed at 8 MHz and connected to PH0-OSC_IN
exactly. until you solder another crystal there in. then set this new frequency in Cube!