cancel
Showing results for 
Search instead for 
Did you mean: 

whats the use of PPS pin (ETH_pps_out) in Ethernet

VChau
Associate II

Hi all,

I'm working on Ethernet interface with STM32F417, I Generate the code by cubeMx for Ethernet stack (lwip).

I want to know whats the use of PPS (ETH_pps_out - PB5) in ethernet because neither this pin is connected with phy nor ethernet port rf45.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Javier1
Principal

https://community.st.com/s/question/0D50X00009Xkgx3SAB/eth-pps-signal-generation-in-pf10

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/
LCE
Principal II

It has absolutely nothing to do with the ethernet hardware interface.

It is an output for use with the PTP / 1588v2 synchronization protocol, PPS is the "Pulse Per Second" kinda divided PTP clock output (derived from the PTP registers).

It can be used for evaluation (comparing several synchronized devices), or for further synchronization purposes.