User Activity

Hi All,The idea, to use variable length data on UART receiver is that "Use a timer ",I am using a timer with interrupt, Once the first byte is received timer start and on second byte receive timer STOP and store the data and start the time again, At ...
Hi all,I'm working on Ethernet interface with STM32F417, I Generate the code by cubeMx for Ethernet stack (lwip).I want to know whats the use of PPS (ETH_pps_out - PB5) in ethernet because neither this pin is connected with phy nor ethernet port rf45...
HI All,How to test Stack Over flow in Keil (STM32L0)Is there any document ? or any process to test Stack over flow
Hi All,I want to ask "is it possible to run BLUENRG-355 on internal oscillator (64Mhz) "As per data sheet it supports internal HSI but device firmware says HSE only. /* High speed crystal configuration: BlueNRG-LP supports only HSE 32 MHz */ SystemTi...
I''m working on STM32WL55 series microcontroller and I want to use KEIL IDE,Please let me know does keil support STM32WL55 for FREE
Kudos from