cancel
Showing results for 
Search instead for 
Did you mean: 

what the meaning of transmit only master ? what the different between half duplex and transmit only master ?

Albatross
Associate II

we want connect PE64904  device ( e wire SPI compatible interface)  to stm32f407  

what is the correct interface 

https://www.psemi.com/pdf/datasheets/pe64102ds.pdf

6 REPLIES 6
Ozone
Lead III

There is nothing to read from this device.

You can use SPI, and ignore the Rx values.

Half duplex basically means sequentially alternating transmission direction. In difference to full duplex, were both appens at the same time.

Both is not relevant for your device, because it is write-only.

Albatross
Associate II

so i need use fullduplex definition or half duplex or transmit master only ?

SaB0tAgE
Associate II

whatever you choose, it will be the same for the application.

Albatross
Associate II

so why you wrote "Both is not relevant for your device"

TDK
Guru

Transmit only master makes the most sense, since that's all you need it to do.

If you feel a post has answered your question, please click "Accept as Solution".
Albatross
Associate II

ok thanks