2020-12-01 12:58 AM
Hello,
It's my first try with Usb directly on an MCU, i used stm32cube mx and code generator to make a first test but when i'm running a simple cdc code i get windows throwing me an error about usb bad descriptor.
I linked my ioc and my usb schematic, i tried with and without the filter inductance(usb connected is just wired to an exti)
Solved! Go to Solution.
2020-12-01 2:17 AM
The D+/D- lines are reversed around TVS1. Also for TVS1 you should use 82400102 from WE or USBLC6-2SC6 from ST.
2020-12-01 1:47 AM
First test with system bootloader if your board enumerates. If yes, the problem is in your code. It not carefully check for hardware errors, bridges, opens, wrong parts etc.
2020-12-01 2:17 AM
The D+/D- lines are reversed around TVS1. Also for TVS1 you should use 82400102 from WE or USBLC6-2SC6 from ST.
2020-12-01 2:51 AM
And they should be directly connected!
2020-12-01 3:37 AM
the lines was reversed, very dumb mistake, i'm able to use bootloader and cube mx example, thanks.
thanks for the tip for tvs @Piranha , this device will be in an industrial environement direct connection seems little dangerous isn't it ?
I'm not a huge fan of ST's Hal, what do you guy's use for interact with usb ?
2021-01-16 9:38 AM
I've not used USB stacks till now, but it looks like TinyUSB is getting traction.