cancel
Showing results for 
Search instead for 
Did you mean: 

Validation on target hal driver error

I tried to validate on desktop... an ai model but ended with this error...

Pinagadi_Meghana_0-1741860214520.png

please help me with this error

9 REPLIES 9
Andrew Neil
Super User

@Pinagadi_Meghana wrote:

I tried to validate on desktop


But the thread title says "on target" - so which is it?

 


@Pinagadi_Meghana wrote:
AndrewNeil_0-1741861538398.png

So it's telling you that it can't find the file stm32h7xx.h

Therefore you need to check two things:

  1. Does that file actually exist anywhere in your project?
    If not, then that obviously explains why the compiler can't find it!
     
  2. If it does exist, is it in a location where the compiler will find it?
    ie, are you Include Paths correctly configured?

 

BTW: it's better to post the error messages as text - rather than an image:

https://community.st.com/t5/community-guidelines/how-to-insert-source-code/tac-p/752812/highlight/true#M59

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Sorry... It is validation on target only...
the error message is

Building project
Generating project
Temporary project loaded
Temporary AI configuration done
Generating temporary project code
Building project
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/arm-none-eabi-gcc -c -mcpu=cortex-m7 -mfpu=fpv5-d16 -mfloat-abi=hard  -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_NUCLEO_64 -DUSE_HAL_DRIVER -DSTM32H753xx -D  -IDrivers/CMSIS/Device/ST/STM32H7xx/Include -IDrivers/CMSIS/Include -IDrivers/STM32H7xx_HAL_Driver/Inc/Legacy -IDrivers/STM32H7xx_HAL_Driver/Inc -IInc -IMiddlewares/ST/AI/Inc -O3  -Wall -fdata-sections -ffunction-sections Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.c -o Debug/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.o
<command-line>: error: macro names must be identifiers
In file included from Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal_rcc.h:27,
                 from Inc/stm32h7xx_hal_conf.h:246,
                 from Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal.h:29,
                 from Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.c:36:
Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal_def.h:29:10: fatal error: stm32h7xx.h: No such file or directory
   29 | #include "stm32h7xx.h"
      |          ^~~~~~~~~~~~~
compilation terminated.
make: *** [Makefile:76: Debug/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.o] Error 1
Automatic build and run failed

Everything looks like perfect sir...
still i am facing that issue..

Pinagadi_Meghana_0-1741876587673.png

 

You haven't answered @Andrew Neil 's questions - does that file exist?  It normally lives in the Drivers/CMSIS/Device/ST/STM32H7xx/Include directory.  It the file IS there, can you open it with an editor?  That would check for strange file access attributes.

Pinagadi_Meghana_1-1741878319311.png

Everything looks like perfect sir...
still i am facing that issue..

yes sir it is there

Pinagadi_Meghana_0-1741879284935.png

 

But did you try to open it with some editor like the IDE or Notepad (looks like you are on a Windows PC)?  Like I said, maybe there is a permissions issue (somehow) with that file.

Yes sir... i did that also.... it is opened in text editor...

I will share my file... please solve that hal drivers errors.... or any other errors during build all...
please