2020-04-15 7:52 AM
Hi
I'm very new to STM32. I create a project with STM32CubeMX for the STM32F746-Disco board and I need to use USB OTG HS for sending data to PC through VCP. The data size which I need to send to PC is 24576 Bytes. The USB connected properly but after some second the send data became corrupted! I mean that the data did not send true, Although the USB connection still is established.
Is there a way to solve this problem?
2020-04-16 1:53 PM
Many possibilities... Most likely it´s a fifo speed problem. Maybe try dma transfer