UDP Echo server not working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-08 12:16 AM
Working on a basic UDP Echo server with STM32F429ZI. I had CubeMX add lwIP into the project, but its doesn't seem to receive any packets when I send them. DHCP seems to work as I can see an IP getting assigned on the router.
void udp_echoserver_receive_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p, struct ip_addr *addr, u16_t port)
{
/* Connect to the remote client */
udp_connect(upcb, addr, UDP_CLIENT_PORT);
/* Tell the client that we have accepted it */
udp_send(upcb, p);
/* free the UDP connection, so we can accept new clients */
udp_disconnect(upcb);
/* Free the p buffer */
pbuf_free(p);
}
/**
* @brief Initialize the server application.
* @param None
* @retval None
*/
void udp_echoserver_init(void)
{
struct udp_pcb *upcb;
err_t err;
/* Create a new UDP control block */
upcb = udp_new();
if (upcb)
{
/* Bind the upcb to the UDP_PORT port */
/* Using IP_ADDR_ANY allow the upcb to be used by any local interface */
err = udp_bind(upcb, IP_ADDR_ANY, UDP_SERVER_PORT);
if(err == ERR_OK)
{
/* Set a receive callback for the upcb */
udp_recv(upcb, udp_echoserver_receive_callback, NULL);
}
}
}
These are my init and callback functions. In main I call ethernetif_input(&gnetif);
I'd like to store the packets to be read in main using the RxCmpltCallback, but I'm not sure what to do. Also despite ICMP being enabled, no pings are recieved when I use a ping program.
Solved! Go to Solution.
- Labels:
-
Ethernet
-
STM32CubeMX
-
STM32F4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-09 8:56 PM
Turns out that the setup for the Nucleo and non-Nucleo chips are different for the PHY address. Changed PHY address to 0 and everything started working. (For anyone wondering, PHY address is declared in stm32f4xx_hal_conf.h, or use CubeMX if you already are.)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-08 3:47 PM
I switched to using MX_LWIP_Process(); instead of ethernetif_input(&gnetif);
I also had a suspicion that I was not actually having a full connection to the interface, as if the router was assigning an IP whether it was requested or not. I commented out MX_LWIP_Init() and my udp_echoserver_init(). An IP was still assigned, so it must be something with the interface initialization. That's my thought at the moment.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-05-09 8:56 PM
Turns out that the setup for the Nucleo and non-Nucleo chips are different for the PHY address. Changed PHY address to 0 and everything started working. (For anyone wondering, PHY address is declared in stm32f4xx_hal_conf.h, or use CubeMX if you already are.)