cancel
Showing results for 
Search instead for 
Did you mean: 

The latest Cubemx update (5.2.0) cannot open ioc files from version 5.1.0 [SOLVED]

wj.anggara
Associate II

Dear ST,

I have problems when opening files with the .ioc extension from the previous cubemx version (5.1.0) on the latest cubemx release (5.2.0), after confirmation of installing the package needed but the file is not open but only loading forever.

Thank you for the support

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
PGogt
Associate III

Hey I have the same problem. This topic is marked solved. How did you solve this?

wj.anggara
Associate II

To solve this problem simply start "ACCESS TO MCU SELECTOR" then select the series of chips that must be loaded manually. After selecting the chip, click "Start Project" then click File -> Load Project ... Select the file with the .ioc extension that you want to open.

PGogt
Associate III

Thanks wj.anggara. It worked spot on. Weird but it works.

wj.anggara
Associate II

Yes. You're welcome @PGogt​ , happy coding :smiling_face_with_smiling_eyes: