cancel
Showing results for 
Search instead for 
Did you mean: 

tooltips in .ioc file view disappear or appear randomly

chriskuku
Senior II

When having those yellow /!\-info icons beside entries, like in the picture below,

it is hard to catch them by hovering over them. They pop up too short to read them. (macOS BigSur in this case, Apple mouse) How can I read what's in there?

1 REPLY 1
chriskuku
Senior II

Somehow I managed while hovering over the PA0-pin that the issue was that

PA0 has a function "PA0_WKUP" programmed while it was additionally configured as GPIO-output pin for my application. How can I resolve this conflict?

The tooltip there at the pin says "holding down CTRL + left mouse button " to show alternate pins.

Doing that it doesn't show anything. (It's a Mac keyboard, so is CTRL maybe CMD?)