Timer interrupt issue with CubeMX generated code, NucleoF722ZE board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 12:38 PM
NucleoF722ZE board, Stm32CubeMX ver 4.22.1, Eclipse
Version: Neon.3 Release (4.6.3)
I wanted to setup TIM6 as timer interrupt for 400usec sampling loop. In CubeMX : TIM6 clocked at 1Mhz and ARR = 400,
TIM6 Configuration/NVIC settings/Enabled (TIM6 global interrupt), then in NVIC Configuration/enabled TIM6 global interrupt with Preemp Priority=10 and Sub Priority=0. Then Generate code.
The generated code seemed to be OK, and it also had
set NVIC interrupt priority and enable as below.
HAL_NVIC_SetPriority(
TIM6_DAC_IRQn, 10, 0);
HAL_NVIC_EnableIRQ(
TIM6_DAC_IRQn);
I added code to toggle the LED inside the ISR void TIM6_DAC_IRQHandler (void) and it never triggered.
Result:
TIM6 was counting OK (read TIM6.CNT and outputted on PWM pin for monitoring), but there was no timer overflow interrupt generated.
However after adding TIM6.DIER = 1; // DMA/interrupt enable, then it worked.
What I need to add TIM6.DIER=1; instead of by CubeMX? or what I did wrong in my steps?
Thanks,
Brian
#stme32-cube #timer-interrupts #cubemx-4.22Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
TIM
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 3:41 PM
Hello!
Did you start the timebase by calling HAL_TIM_Base_Start_IT or HAL_TIM_Base_Start_DMA(in case you use DMA)?
Also 400 microsecond is very short time to observe toggling by eye.
Regards
vf
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 3:41 PM
Hello!
Did you start the timebase by calling HAL_TIM_Base_Start_IT or HAL_TIM_Base_Start_DMA(in case you use DMA)?
Also 400 microsecond is very short time to observe toggling by eye.
Regards
vf
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-13 4:45 PM
Hi VF,
Thanks for the answer. No, I didn't use those functions; to start the timer I just set the bit CE=1 in the CR1 register. I was aware that one needed to call HAL_TIM_Base_Start(TIM6) for the timer to run from reading other posts, but I didn't know those functions mentioned by you exist. How do I know they are exist and how to use them?
So I searched for
HAL_TIM_Base_Start_IT, and this answers my question. It calls a macro to set the interrupt bit in TIM6.DIER register.
Thanks,
Brian
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-14 5:00 AM
Hi Brian.
Unfortunately there is not detailed documentation to read from.
There is a description only at HAL user manual inside HAL firmware at \STM32Cube\Repository\STM32Cube_FW_F7_V1.7.0\Drivers\STM32F7xx_HAL_Driver.
Take a look also inside stm32f7xx_hal_tim.c module. In the begining there is a summary of all tim functions and their use
You can study also every function inside modules to havean idea how it works.
Regards
vf