2021-05-19 5:24 PM
EXTI12 implies that the ARM external interrupt that is triggered is EXTI15_10_IRQn, when actually this pin triggers the EXTI2 interrupt. I think the issue is with the STM32Cube IDE code generator for this particular family of boards. (I tried to use EXTI2 as a software interrupt but when I touched the board in certain places it would cause my code to hang --- well, I thought this vector was available since I didn't see it being used in the configuration tool :) ). I've since solved this minor issue for myself but thought I should share it with ST.
/*Configure GPIO pin : PMOD_IRQ_EXTI12_Pin */
GPIO_InitStruct.Pin = PMOD_IRQ_EXTI12_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(PMOD_IRQ_EXTI12_GPIO_Port, &GPIO_InitStruct);
I think should be:
/*Configure GPIO pin : PMOD_IRQ_EXTI2_Pin */
GPIO_InitStruct.Pin = PMOD_IRQ_EXTI2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(PMOD_IRQ_EXTI12_GPIO_Port, &GPIO_InitStruct);
2021-06-04 6:32 AM
Hello @MNeed.1
Thank you for your post,
I'll check it then I'll get back to you :)
Khouloud
2021-06-04 6:46 AM
Hi again @MNeed.1
You're right, I confirm the issue and it will be fixed.
Many thanks for bringing this problem to our attention and for your contribution :)
Khouloud