2025-03-09 10:59 PM
Hi Team,
Please help add support for MDK-ARM version 6.22. Currently highest selectable Min Version is V5.32
Thanks in advance.
2025-03-09 11:13 PM
no issue .... you can generate your project in 5.32 and you can open it in the higher version of MDK-ARM
2025-03-09 11:26 PM - edited 2025-03-09 11:30 PM
2025-03-09 11:42 PM
in the code generation select ARM Compiler option as "Use Default Compiler version 5". after doing this if you'll get same errors then you need to download version 5 compiler from keil website.
2025-03-09 11:45 PM
I can compile using version 5, but I need help building an example for compiler version 6.