2020-03-22 11:35 PM
When I created a new project using the stm32cubeide, and set the new project to be able to go to standby mode and then wakeup using RTC timer, it works.
But when I try to add the standby mode with RTC Wakeup timer to a pre-existing example project, I can't seem to be able to wakeup from sleep but I am using the same configurations that I use in the new/blank project.
For Context, I am using the HAL Libraries to produce the standby mode and RTC Wakeup timer and adding it to the fp-ind-predmnt1 example project of ST, is there anything that I missed doing to configure the example project? also this example project doesn't have ioc so I don't know to configure anything that needs stm32cubemx ioc files
2020-03-23 3:05 AM
Hello @reokyouma
have you added the code for enabling the WakeUp ?
Regards,
Nesrine
2020-03-23 3:28 AM
am i right to assume this one ?
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);I tried it but It didn't work out
uint8_t predrun =0;
int main(void)
{
HAL_Init();
HAL_PWREx_EnableVddIO2();
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddUSB();
/* Configure the System clock */
SystemClock_Config();
RTC_init();
if(__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET){
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc,RTC_FLAG_ALRAF);
}
predrun =0;
InitTargetPlatform(TARGET_STWIN);
t_stwin = HAL_GetTick();
/* For enabling CRC clock for using motion libraries (for checking if STM32 microprocessor is used)*/
MX_CRC_Init();
/* Check the MetaDataManager */
InitMetaDataManager((void *)&known_MetaData,MDM_DATA_TYPE_GMD,NULL);
PREDMNT1_PRINTF("\n\t(HAL %ld.%ld.%ld_%ld)\r\n"
"\tCompiled %s %s"
#if defined (__IAR_SYSTEMS_ICC__)
" (IAR)\r\n"
#elif defined (__CC_ARM)
" (KEIL)\r\n"
#elif defined (__GNUC__)
" (STM32CubeIDE)\r\n"
#endif
"\tSend Every %4dmS Temperature/Humidity/Pressure\r\n"
"\tSend Every %4dmS Acc/Gyro/Magneto\r\n"
"\tSend Every %4dmS dB noise\r\n\n",
HAL_GetHalVersion() >>24,
(HAL_GetHalVersion() >>16)&0xFF,
(HAL_GetHalVersion() >> 8)&0xFF,
HAL_GetHalVersion() &0xFF,
__DATE__,__TIME__,
PERIOD_ENVIRONMENTAL,
PERIOD_ACC_GYRO_MAG,
MICS_DB_UPDATE_MUL_10MS * 10);
#ifdef PREDMNT1_DEBUG_CONNECTION
PREDMNT1_PRINTF("Debug Connection Enabled\r\n");
#endif /* PREDMNT1_DEBUG_CONNECTION */
#ifdef PREDMNT1_DEBUG_NOTIFY_TRAMISSION
PREDMNT1_PRINTF("Debug Notify Trasmission Enabled\r\n\n");
#endif /* PREDMNT1_DEBUG_NOTIFY_TRAMISSION */
/* Set Node Name */
ReCallNodeNameFromMemory();
HCI_TL_SPI_Reset();
/* Initialize the BlueNRG */
Init_BlueNRG_Stack();
/* Initialize the BlueNRG Custom services */
Init_BlueNRG_Custom_Services();
/* Check the BootLoader Compliance */
PREDMNT1_PRINTF("\r\n");
if(CheckBootLoaderCompliance()) {
PREDMNT1_PRINTF("BootLoader Compliant with FOTA procedure\r\n\n");
} else {
PREDMNT1_PRINTF("ERROR: BootLoader NOT Compliant with FOTA procedure\r\n\n");
}
/* Set Accelerometer Full Scale to 2G */
Set2GAccelerometerFullScale();
/* initialize timers */
InitTimers();
/* Predictive Maintenance Initialization */
InitPredictiveMaintenance();
/* Infinite loop */
while (1)
{
/* Led Blinking when there is not a client connected */
if(!connected)
{
if(!TargetBoardFeatures.LedStatus) {
if(!(HAL_GetTick()&0x3FF)) {
LedOnTargetPlatform();
}
} else {
if(!(HAL_GetTick()&0x3F)) {
LedOffTargetPlatform();
}
}
}
if(set_connectable){
if(NecessityToSaveMetaDataManager) {
uint32_t Success = EraseMetaDataManager();
if(Success) {
SaveMetaDataManager();
}
}
/* Now update the BLE advertize data and make the Board connectable */
setConnectable();
set_connectable = FALSE;
}
/* Handle user button */
if(ButtonPressed) {
ButtonCallback();
ButtonPressed=0;
}
if(PredictiveMaintenance){
if (IsFirstTime)
{
IsFirstTime = 0;
/* Initializes the MotionSP Vibration parameters */
MotionSP_VibrationInit();
if(FFT_Alarm)
{
/* Initialization of Alarm Status on Axes, Alarm Values Reported
and Thresholds to detect WARNING and ALARM conditions */
MotionSP_TimeDomainAlarmInit(&sTdAlarm, &sTimeDomainVal, &sTdRmsThresholds, &sTdPkThresholds);
/* Frequency domain initialization of Alarm Status */
MotionSP_FreqDomainAlarmInit(&FDWarnThresh, &FDAlarmThresh, &THR_Fft_Alarms, MotionSP_Parameters.subrange_num);
}
/* Configure the FIFO settings in according with others parammeters changed */
MotionSP_ConfigFifo();
enable_FIFO();
/* Start of the Time Window */
Start_Tick = HAL_GetTick();
}
MotionSP_VibrationAnalysis();
predrun=1;
}
/* handle BLE event */
if(HCI_ProcessEvent) {
HCI_ProcessEvent=0;
hci_user_evt_proc();
}
/* Environmental Data */
if(SendEnv) {
SendEnv=0;
SendEnvironmentalData();
}
/* Mic Data */
if (SendAudioLevel) {
SendAudioLevel = 0;
SendAudioLevelData();
}
/* Motion Data */
if(SendAccGyroMag) {
SendAccGyroMag=0;
SendMotionData();
}
/* Battery Info Data */
if(SendBatteryInfo){
SendBatteryInfo=0;
SendBatteryInfoData();
}
if(!connected && predrun == 1){
predrun=0;
RTC_CalendarConfig();
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc,RTC_FLAG_ALRAF);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
RTC_AlarmConfig();
// HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xFFFF, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
HAL_PWR_EnterSTANDBYMode();
}
/* Wait for Event */
//__WFI();
}
}
void RTC_init(void){
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_12;
hrtc.Init.AsynchPrediv = 0x7F;
hrtc.Init.SynchPrediv = 0xFF;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if(HAL_RTC_Init(&hrtc) != HAL_OK){
Error_Handler();
}
}
void RTC_CalendarConfig(void){
//this function does the rtc calendar config
RTC_TimeTypeDef RTC_TimeInit;
RTC_TimeInit.Hours = 12;
RTC_TimeInit.Minutes = 11;
RTC_TimeInit.Seconds = 0;
RTC_TimeInit.TimeFormat = RTC_HOURFORMAT12_AM;
HAL_RTC_SetTime(&hrtc, &RTC_TimeInit, RTC_FORMAT_BIN);
RTC_DateTypeDef RTC_DateInit;
RTC_DateInit.Date = 12;
RTC_DateInit.Month = RTC_MONTH_JUNE;
RTC_DateInit.Year = 18;
RTC_DateInit.WeekDay = RTC_WEEKDAY_TUESDAY;
HAL_RTC_SetDate(&hrtc, &RTC_DateInit, RTC_FORMAT_BIN);
}
void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{
/* Prevent unused argument(s) compilation warning */
// UNUSED(hrtc);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_RTC_AlarmAEventCallback could be implemented in the user file
*/
}
void RTC_AlarmConfig(void){
RTC_AlarmTypeDef RTC_AlarmInit;
memset(&RTC_AlarmInit,0,sizeof(RTC_AlarmInit));
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
RTC_AlarmInit.Alarm = RTC_ALARM_A;
RTC_AlarmInit.AlarmTime.Hours = 12;
RTC_AlarmInit.AlarmTime.Minutes = 11;
RTC_AlarmInit.AlarmTime.Seconds=10;
RTC_AlarmInit.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM;
RTC_AlarmInit.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY;
RTC_AlarmInit.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_NONE;
if(HAL_RTC_SetAlarm(&hrtc, &RTC_AlarmInit, RTC_FORMAT_BIN) != HAL_OK){
Error_Handler();
}
}should be the whole code
2020-03-23 3:35 AM
try this code,
/** Enable the WakeUp
*/
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
{
Error_Handler();
}
2020-03-23 4:20 AM
unfortunately it did't work
Correct me if I am wrong but aside from the code above, I need put this into the msp.c right?
void HAL_RTC_MspInit(RTC_HandleTypeDef* hrtc)
{
//1. turn on LSE
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){
Error_Handler();
}
//2 select LSE as RTC CLK
RCC_PeriphCLKInitTypeDef RCC_RTCPeriphCLKInit;
RCC_RTCPeriphCLKInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
RCC_RTCPeriphCLKInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if(HAL_RCCEx_PeriphCLKConfig(&RCC_RTCPeriphCLKInit) != HAL_OK){
Error_Handler();
}
// 3 Enable the RTC Clock
__HAL_RCC_RTC_ENABLE();
//4 enable interrupt
HAL_NVIC_SetPriority(RTC_Alarm_IRQn,15,0);
HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);
}
/**
* @brief RTC MSP De-Initialization
* This function freeze the hardware resources used in this example
* @param hrtc: RTC handle pointer
* @retval None
*/
void HAL_RTC_MspDeInit(RTC_HandleTypeDef* hrtc)
{
if(hrtc->Instance==RTC)
{
/* USER CODE BEGIN RTC_MspDeInit 0 */
/* USER CODE END RTC_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_RTC_DISABLE();
/* USER CODE BEGIN RTC_MspDeInit 1 */
/* USER CODE END RTC_MspDeInit 1 */
}
}and this one to the it.c
void RTC_Alarm_IRQHandler(void){
HAL_RTC_AlarmIRQHandler(&hrtc);
}