cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7R7L8H6 - CubeMX Config - I2C1 and I3C Not working?

Uman-Butani
Associate II

Dear Team, 
When I am starting a new project in cube MX with STM32H7R7L8H6, there are options of I2C1 and I3C1. but I am not able to select and make it work. drop-down menu is not enabled!
I am using V 6.12.0
 

UmanButani_0-1720775430307.png

Does anyone have any explanation for this? 

Regards
Umang

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Uman-Butani 

You just have to enable the flash on the same context that you are looking to select for the I2C or the I2S (Boot or Application):

STTwo32_0-1720776476917.png

 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @Uman-Butani 

You just have to enable the flash on the same context that you are looking to select for the I2C or the I2S (Boot or Application):

STTwo32_0-1720776476917.png

 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.