cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7B0VB Max Clock

MMira.4
Associate

Hi, I'm trying to configure my stm32h7b0vb for max clock (280Mhz), but max freq on DIVN1 is 420Mhz, and DIVP1 is 2 (min val). Therefore I only reach 210Mhz

0693W00000Kbff4QAB.png

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

DIV1M can be less than /16. Here is one of several working scenarios:

0693W00000Kbg2cQAB.png 

Make sure you have VOS0 selected in RCC -> Power Parameters.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

DIV1M can be less than /16. Here is one of several working scenarios:

0693W00000Kbg2cQAB.png 

Make sure you have VOS0 selected in RCC -> Power Parameters.

If you feel a post has answered your question, please click "Accept as Solution".
MMira.4
Associate

Thanks, I was trying to use DIV1M between 1-2Mhz!

Yeah, I think that was desirable for the PLL comparison frequency on the F2/F4 parts, but a lot of the H7 I typically see 5 MHz

I'd like to see ST provide characterization charts for the overall stability, but I've been disappointed for over a decade..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..