cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 use various uart the code sending is change

wjian.2
Associate III

if i normolly send is "cake 50 %" to arduino receive "cake 50 %" after 10 times arduino receive "cake 50 BBBB" then all receive all "BBBC" but the usart1 vcp is sending normally this is a way to solve it?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Karl Yamashita
Principal

Post your code so we can see what you're doing

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source