2020-08-27 11:44 AM
To reproduce: generate a project using ADC3 with the LL driver on STM32CubeMX 6.0.1.
Issue: regardless of which ADC is used, this shows up in MX_ADCx_Init():
/* Disable ADC deep power down (enabled by default after reset state) */
LL_ADC_DisableDeepPowerDown(ADC1);
/* Enable ADC internal voltage regulator */
LL_ADC_EnableInternalRegulator(ADC1);The issue appears to stem from db/mcu/config/llConfig/ADC-STM32G4xx_LLConfigs.xml:
<CallLibMethod Name="" Type="HardCode">
<HardCode Text="
#n#t/* Disable ADC deep power down (enabled by default after reset state) */
#n#tLL_ADC_DisableDeepPowerDown(ADC1);
#n#t/* Enable ADC internal voltage regulator */
#n#tLL_ADC_EnableInternalRegulator(ADC1);
#n#t/* Delay for ADC internal voltage regulator stabilization. */
#n#t/* Compute number of CPU cycles to wait for, from delay in us. */
#n#t/* Note: Variable divided by 2 to compensate partially */
#n#t/* CPU processing cycles (depends on compilation optimization). */
#n#t/* Note: If system core clock frequency is below 200kHz, wait time */
#n#t/* is only a few CPU processing cycles. */
#n#tuint32_t wait_loop_index;
#n#twait_loop_index = ((LL_ADC_DELAY_INTERNAL_REGUL_STAB_US * (SystemCoreClock / (100000 * 2))) / 10);
#n#twhile(wait_loop_index != 0)
#n#t{
#n#t#twait_loop_index--;
#n#t}"
/>
</CallLibMethod>It appears that ADC1 is hard-coded into the config XML file. I have to manually edit the code to ADC3 after generation to fix this issue.
2020-09-25 2:55 AM
Hi @GLi.3 ,
Unfortunately your post was missed simply because it was misplaced under Bug-report topic. There are more opportunities to review it if you used topics STM32CubeMX and STM32G4.
Any way, for this one: I report it to our development team in order to take relevant corrective actions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-09-25 3:27 AM
Hello GLi.3,
Sorry for the inconvenience, it is a known issue and it has been already reported to STM32CubeMX development team to be fixed. The fix will be available in the future release. Thanks for your patience.
Regards,
Khouloud.