STM32f446RE Timer6 DMA problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-13 9:08 AM
Hello All,
I have some serious issue which i am not able to figure it out, i really dont know what i am missing,
basically what i am doing is simple,
i m using TIM6 (BASIC TIMER) dma to toggle the led.
The problem is , the moment i trigger the dma it goes to 'Transfer Error' block of the DMA isr,
i have no clue why this is happening , below is my code, i must be doing something silly, but i spent 2 days , i have no clue
&sharpinclude<stdio.h>
&sharpinclude 'stm32f446xx.h'/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim6;DMA_HandleTypeDef hdma_tim6_up;uint8_t data[2]={0xff,0x00};
/* Private function prototypes -----------------------------------------------*/void SystemClock_Config(void);static void MX_GPIO_Init(void);
static void MX_TIM6_Init(void);
static void MX_DMA_init(void);int main()
{ SystemClock_Config(); MX_GPIO_Init();MX_TIM6_Init();
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();/* DMA interrupt init */
/* DMA1_Stream1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);MX_DMA_init();
__HAL_TIM_ENABLE_DMA(&htim6, TIM_DMA_UPDATE); HAL_NVIC_SetPriority(TIM6_DAC_IRQn, 0, 0); HAL_NVIC_EnableIRQ(TIM6_DAC_IRQn);HAL_DMA_Start_IT(htim6.hdma[TIM_DMA_ID_UPDATE], (uint32_t)&data, (uint32_t)&GPIOA->ODR, 2);
HAL_TIM_Base_Start(&htim6); //trigger the timer.
while(1);
}void MX_DMA_init(void){ /* Peripheral DMA init*/ hdma_tim6_up.Instance = DMA1_Stream1; hdma_tim6_up.Init.Channel = DMA_CHANNEL_7; hdma_tim6_up.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_tim6_up.Init.PeriphInc = DMA_PINC_DISABLE; hdma_tim6_up.Init.MemInc = DMA_MINC_ENABLE; hdma_tim6_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_tim6_up.Init.MemDataAlignment = DMA_PDATAALIGN_BYTE; hdma_tim6_up.Init.Mode = DMA_CIRCULAR; hdma_tim6_up.Init.Priority = DMA_PRIORITY_HIGH; hdma_tim6_up.Init.FIFOMode = DMA_FIFOMODE_DISABLE; if (HAL_DMA_Init(&hdma_tim6_up) != HAL_OK) { while(1); }__HAL_LINKDMA(&htim6,hdma[TIM_DMA_ID_UPDATE],hdma_tim6_up);
}/** System Clock Configuration*/void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;/**Configure the main internal regulator output voltage
*/ __HAL_RCC_PWR_CLK_ENABLE();__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 96; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { while(1); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV4;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{ while(1); }}/* TIM6 init function */static void MX_TIM6_Init(void){TIM_MasterConfigTypeDef sMasterConfig;
__HAL_RCC_TIM6_CLK_ENABLE();htim6.Instance = TIM6;
htim6.Init.Prescaler = 47999; htim6.Init.CounterMode = TIM_COUNTERMODE_UP; htim6.Init.Period = 500; if (HAL_TIM_Base_Init(&htim6) != HAL_OK) { while(1); }&sharpif 1
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK) { while(1); } &sharpendif}
/** Configure pins as
* Analog * Input * Output * EVENT_OUT * EXTI PA2 ------> USART2_TX PA3 ------> USART2_RX*/static void MX_GPIO_Init(void){GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin : LD2_Pin */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}
/*** @brief This function handles TIM6 global interrupt and DAC1, DAC2 underrun error interrupts.*/void TIM6_DAC_IRQHandler(void){ /* USER CODE BEGIN TIM6_DAC_IRQn 0 *//* USER CODE END TIM6_DAC_IRQn 0 */
HAL_TIM_IRQHandler(&htim6); /* USER CODE BEGIN TIM6_DAC_IRQn 1 *//* USER CODE END TIM6_DAC_IRQn 1 */
}/*** @brief This function handles DMA1 stream1 global interrupt.*/void DMA1_Stream1_IRQHandler(void){ /* USER CODE BEGIN DMA1_Stream1_IRQn 0 *//* USER CODE END DMA1_Stream1_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_tim6_up); /* USER CODE BEGIN DMA1_Stream1_IRQn 1 *//* USER CODE END DMA1_Stream1_IRQn 1 */
}#smt32f4-cubemx #dma-stm32- Labels:
-
DMA
-
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-13 9:38 AM
You'd need to use DMA2 and a timer on APB2 for your copy from memory to memory to succeed.
GPIOA->ODR is classed as a memory transaction as it is on the AHB, not APB1 or APB2
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-13 7:24 PM
Many Thanks
turvey.clive
‌ , somehow i ignored this, i am going to try this today . Thanks again.