2018-09-06 06:22 PM
HI, There .
I bought STM32F429I-DISC1 evaluation board.
In first. I download demonstration firmware.
\STM32Cube_FW_F4_V1.21.0\Projects\STM32F429I-Discovery\Demonstrations\STemWin
Run that . feel so good .ST-LINK is active and I can see USB Mass storage.
but not responsed when USB USER connected(CN6).
and freeze when I chooose FileViewer in top nemu.
I think 1more mass storage confirm when USB USER connect.Is it misunderstand?
I checked device manager in windows.it is host of USB.
unknown device was detected.Need I get driver for that device??
Pls help me. How to resolve it or where check ?
Thanks in advance.
2018-09-06 06:46 PM
device id of unknown device
USB\VID_0483&PID_374B&REV_0100&MI_02
2018-09-07 02:37 PM
Device USB\VID_0483&PID_374B&REV_0100 is the STLink debugger.
The driver for it is available on ST.com.
It has several variants, your variant seems to be a multifunction device and the other function is likely a "virtual COM port".
-- pa