2019-02-26 11:50 AM
I opened an older project which was created with 5.0.1, and the newest CubeMX shows an error for this option in ADC. But this option is correct. I tried to create a new project, and I wasn't able to enable this option here.
Solved! Go to Solution.
2019-04-24 1:11 AM
So it means, this issue is fixed too? It's mainly related to low layer driver, with HAL it worked before.
2019-04-24 4:14 PM
2019-04-25 12:08 AM
@Jeff Gros
You're Right, this issue is already reported and it wil be fixed in the next release. Sorry for any inconvenience this may have brought.
Best Regards
khouloud.
2019-04-26 12:09 AM
Yes, this is fixed. I can confirm it too!
But you can't measure temp sensor with vref with LL, because freshly generated code will only enable measuring vrefint. Tested with 5.2.0.
2019-08-06 6:42 AM
Hello I was working in Mxcube 5.01 and I updated to 5.3.0 and I can not set the parameter DMA continues Request to ENABLE only Disable shows up.
I was using and project that I am working, but I created a new one from the scratch and I can no set this option. I ma using STM32F446ZEJx.
Is this bug not fixed for this MCU ?
Thank you
2019-08-06 6:52 AM
When I open my old Project I clicked in migrate project, I got my old Ioc file and I did not click Migrate I just clicked in Download package and this allow me to change this DAM setting, but if i do i new project I can not change it using STM32F446ZEJx
Thank you
2019-08-06 7:25 AM
hello @mospi , I will check it, please share your ioc file.
Best Regards,
Khouloud.
2019-08-07 9:44 AM
2019-09-03 5:23 AM
I have the same problem with SMT32F446RE.
2019-09-03 6:30 AM
Hello the Ioc was shared like month ago.
can you tell us if this bug is fixed or how can we go around this.
Thank you