2018-09-14 12:08 AM
STM32CubeMX V4.27.0 release note states that STM32H7 uses firmware V1.4.0. Whereas in reality it uses V1.3.0. Is it possible to download STM32H7 firmware V1.4.0. I could not find it anywhere. Is firmware update planed?
Solved! Go to Solution.
2018-09-18 02:54 AM
Hello @MaxR ,
We are sorry, there is a typo in Release note of STM32CubeMX 4.27.0 , STM32H7 use V1.3.0 and not 1.4.0.
It is not possible to download the H7 FW 1.4.0 because it is not yet available 🙂 but update is planned for the future.
Regards,
Houda
2018-09-14 05:57 AM
Hi @MaxR ,
The STM32H7 uses STM32Cube firmware V1.3.0. This is a typo in the release note which will be fixed in the next update of the document.
Thanks for bringing this point to our attention.
Khouloud.
2018-09-14 08:43 AM
>>Is firmware update planed?
It is, but there isn't a schedule, and current release supports the NUCLEO/EVAL boards fully
2018-09-18 02:54 AM
Hello @MaxR ,
We are sorry, there is a typo in Release note of STM32CubeMX 4.27.0 , STM32H7 use V1.3.0 and not 1.4.0.
It is not possible to download the H7 FW 1.4.0 because it is not yet available 🙂 but update is planned for the future.
Regards,
Houda