cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX project generation have problem BUG on samba

SKape
Associate II

​Hello.

I work on Windows on a network drive.

The file server is samba which, by default, for files whose name starts with a dot, gives the hidden attribute.

After generating the TrueStudio project, the .project and .cproject files are thus given a hidden attribute.

When re-generating the project using CubeMX, the following error appears: '' The Code is fully generated under (mypathname), but TrueSTUDIO project generation have a problem. ''

I can not change file server settings, therefore I am unable to remove the attribute hidden from the .project and .cproject file.

Is it possible the STM32CubeMX will work with the TrueSTUDIO project files that have hidden attributes?

0 REPLIES 0