cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx not working anymore after update from 5.4.0 to 5.5.0

Katzenberger.Michael
Associate III

Hi !

After updating I'm not able to load any project or generating a new one.

Each time a project is loaded the program crashes with

...
2020-01-10 23:34:35,765 [INFO] BlockDiagram:1818 - stop enableDisableButtons
java.lang.NullPointerException
...
at java.desktop/java.awt.EventDispatchThread.run(EventDispatchThread.java:90)
Exception in thread "AWT-EventQueue-0" java.lang.NoSuchMethodError: 'boolean com.st.microxplorer.mcu.IP.isDMASupported()'
...

Please see attached text file for full log.

9 REPLIES 9
dbgarasiya
Senior II

problem is because of jave

please update java first then try

Katzenberger.Michael
Associate III

Thanks for your feedback.

But neither a update of java11 nor installing java13 solves the problem. I've attached the full log of both java versions.

> java --version
openjdk 13 2019-09-17
OpenJDK Runtime Environment (build 13+33)
OpenJDK 64-Bit Server VM (build 13+33, mixed mode, sharing)
> java --version
openjdk 11 2018-09-25
OpenJDK Runtime Environment 18.9 (build 11+28)
OpenJDK 64-Bit Server VM 18.9 (build 11+28, mixed mode)
> lsb_release --all
No LSB modules are available.
Distributor ID:	LinuxMint
Description:	Linux Mint 19.3 Tricia
Release:	19.3
Codename:	tricia

Katzenberger.Michael
Associate III

I was not able to upload both files ?????

So here is the log for java 13

dbgarasiya
Senior II
Katzenberger.Michael
Associate III

you mean this comment, right ?

STM32CubeIDE toolchain:

• It is functional only with a Java 8 64-bit Java Virtual Machine.

I've used this java version in the past (and STM32CubeMX version 5.4.0 was running fine with that):

> java -version
openjdk version "1.8.0_232"
OpenJDK Runtime Environment (build 1.8.0_232-8u232-b09-0ubuntu1~18.04.1-b09)
OpenJDK 64-Bit Server VM (build 25.232-b09, mixed mode)

Although the revision number (?) is 232 I've downloaded the latest available package form java.com which has a revision number of 231

> java -version
java version "1.8.0_231"
Java(TM) SE Runtime Environment (build 1.8.0_231-b11)
Java HotSpot(TM) 64-Bit Server VM (build 25.231-b11, mixed mode)

Unfortunately no improvement ...

And the jdk version is not downloadable without an Oracle account.

So currently all installed versions didn't work:

> sudo update-alternatives --config java
There are 4 choices for the alternative java (providing /usr/bin/java).
 
  Selection    Path                                            Priority   Status
------------------------------------------------------------
  0            /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java   1081      auto mode
  1            /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java   1081      manual mode
  2            /usr/lib/jvm/jdk-11/bin/java                     0         manual mode
  3            /usr/lib/jvm/jdk-13/bin/java                     0         manual mode
* 4            /usr/lib/jvm/jre1.8.0_231/bin/java               0         manual mode
 
Press <enter> to keep the current choice[*], or type selection number: 

Katzenberger.Michael
Associate III

Finally a fresh install of STM32CubeMx solved the problem !

Hi Michael

What java version are you finally using?

Katzenberger.Michael
Associate III

Hi Christian,

obviously the "only Java 8" statement is not true ;-)

I'm running jdk-13

> java -version
openjdk version "13" 2019-09-17
OpenJDK Runtime Environment (build 13+33)
OpenJDK 64-Bit Server VM (build 13+33, mixed mode, sharing)

Thanks for you answer

I have java 8 now and after a clean install of CubeMX 5.5.0, it actually works fine now

$ java -version
openjdk version "1.8.0_242"
OpenJDK Runtime Environment (build 1.8.0_242-8u242-b08-0ubuntu3~18.04-b08)
OpenJDK 64-Bit Server VM (build 25.242-b08, mixed mode)

(I had java 11 before and CubeMX 5.4.0 was working fine with it)