Skip to main content
BCarl
Visitor II
January 18, 2019
Question

STM32CubeMX Generating Code with Licensing Issues

  • January 18, 2019
  • 1 reply
  • 733 views

When selecting "Makefile" for Toolchain/IDE with the STM32F4 Family of MCU's, a Linker Script is generated with a license that does not allow the code to be used with anything other than "System Workbench".

** (c)Copyright Ac6.
** You may use this file as-is or modify it according to the needs of your
** project. Distribution of this file (unmodified or modified) is not
** permitted. Ac6 permit registered System Workbench for MCU users the
** rights to distribute the assembled, compiled & linked contents of this
** file as part of an application binary file, provided that it is built
** using the System Workbench for MCU toolchain.

This topic has been closed for replies.

1 reply

MNapi
Senior II
January 18, 2019

I have been using Cube MX for the last month and Keil. Cube MX would generate all the initialization codes for project and open automatically Keil. I have not seen any problems so far.

As far as I know Cube MX is free to download and use.