2016-12-30 11:52 PM
Hi,
I've created a very simple project in STM32CubeMX for the F3DISCOVERY board. The only things I changed from the default are enabling MCO, and setting the PLL multiplier to When I import the code into SW4STM32 and press build, I get the following error:
17:41:40 **** Build of configuration Debug for project test_64mhz ****
make all
Building file: ../Src/main.c
Invoking: MCU GCC Compiler
/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Debug
arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Device/ST/STM32F3xx/Include' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Include' -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c'
/bin/sh: -c: line 0: syntax error near unexpected token `('
/bin/sh: -c: line 0: `arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Device/ST/STM32F3xx/Include' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Include' -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c''
make: *** [Src/main.o] Error 2
17:41:40 Build Finished (took 94ms)�?�?�?�?�?�?�?�?�?�?�?
My operating system is OSX Yosemite, and both SW4STM32 and STM32CubeMX are updated to the latest versions.
Thanks,
Jeremy
#stm32cubemx #sw4stm322017-03-01 6:33 AM
Hello,
This point is more belong Eclipse plugins.
Could you please go to
http://www.openstm32.org/forums
and open a discussion thread related to this topic ?
Thanks in avance.
Kind regards
Sirma