Thanks @Tesla DeLorean . Works like a breeze even for H735 discovery board. Apparently this deadlock happens if power settings in firmware are different from that of hardware. This issue is most likely to occur when programming the discovery board fo...
Hi @Ghofrane GSOURI ,Thanks for keeping me posted.While 'Save As' works as such, the folder structure still doesn't appear in the browse window either while opening or saving.I think this is specific to the MAC OS version only. I've shifted to windo...
I'm facing the same issue. STM32Cube Programmer hangs on Mac M1 after clicking the 'Connect' button. STM32 Cube IDE and STM32 CubeMX work well. And the same STM32Cube Programmer with the same hardware set-up works without a glitch on a Windows PC.Any...