2021-05-27 10:14 PM
STM32CubeMX project for STM32F407ZG
Firmware pack FW_F4 V1.26.1
generated project : Option for Target -> Linker -> R/O Base, R/W Base is not configurated which cause Image Entry point wrongly set to 0x00008001
2021-06-04 02:30 AM
Hello @TCL.1 ,
Thank you for your post,
Actually, the default setting is taken from "Memory layout of Target Dialog" as it's checked by default, in case you want to change R/O Base and R/W Base, you need to uncheck this parameter.
Could you please give me more details about the problem that you have encountered ?
Thanks, Khouloud