cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.13.0 breaks on STM32H563 .ioc file (Error: not a vaild ioc file)

aw_von
Associate II

Hello ST Community,

 

   I have a project using the H563. I recently upgraded STM32CubeMX from 6.12.0 to 6.13.0.  After upgrading, and attempting to open the .ioc file, the following message is displayed:

MX1.png

 

Regardless if I choose Continue or Migrate, I get the following error message in STM32CubeMX:

MX2.png

 

If I downgrade STM32CubeMX to 6.12.0, I do not get the migration notification pop-up, and the .ioc file opens as expected.  

 

I was hoping to find out why this is occuring and a resolution to it.  I have attached the STM32CubeMX log (which contains both the attempt at Continue and attempt at Migrate, both of which returns the 'not valid ioc file' error), and the .ioc file used.   

Please let me know if additional details or documents are needed.

 

Best regards,

-Aaron Wheeler

1 ACCEPTED SOLUTION

Accepted Solutions
Ghofrane GSOURI
ST Employee

Hello @aw_von @Karl Yamashita 

First let me thank you all for posting.

This behavior is under investigation by development team and tracked by the Ticket 197849  and that will be fixed as soon as possible.

Kind regards
Ghofrane

View solution in original post

3 REPLIES 3
Karl Yamashita
Principal

Using STM32CubeIDE 1.17.0, I get the same error when trying to open your IOC file. 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
Ghofrane GSOURI
ST Employee

Hello @aw_von @Karl Yamashita 

First let me thank you all for posting.

This behavior is under investigation by development team and tracked by the Ticket 197849  and that will be fixed as soon as possible.

Kind regards
Ghofrane

MFuch.3
Associate II

Hello,

how/where can I track that ticket 197849. I have exactly the same with with an STM32H5 ioc file while migrating between the above versions.

Best regards,

Matthias