2024-12-09 12:18 PM
Hello ST Community,
I have a project using the H563. I recently upgraded STM32CubeMX from 6.12.0 to 6.13.0. After upgrading, and attempting to open the .ioc file, the following message is displayed:
Regardless if I choose Continue or Migrate, I get the following error message in STM32CubeMX:
If I downgrade STM32CubeMX to 6.12.0, I do not get the migration notification pop-up, and the .ioc file opens as expected.
I was hoping to find out why this is occuring and a resolution to it. I have attached the STM32CubeMX log (which contains both the attempt at Continue and attempt at Migrate, both of which returns the 'not valid ioc file' error), and the .ioc file used.
Please let me know if additional details or documents are needed.
Best regards,
-Aaron Wheeler
2024-12-09 02:45 PM
Using STM32CubeIDE 1.17.0, I get the same error when trying to open your IOC file.
2024-12-10 12:37 AM - last edited on 2024-12-11 09:08 AM by Semer CHERNI
Hello @aw_von @Karl Yamashita
First let me thank you all for posting.
This behavior is under investigation by development team and tracked by the Ticket 197849 and that will be fixed as soon as possible.
Kind regards
Ghofrane