2020-11-18 7:48 AM
What is new in STM32CubeMX V6.1.0?
Videos
A new thread has been created to gather your requests for Video Tutorials.
If you need to add A Video tutorial or have and idea about a tutorial, don't hesitate to visit the thread below and add your request in a comment.
Added support
• Added the support for new part numbers in the STM32G0 Series:
STM32G0B0CETx, STM32G0B0KETx, STM32G0B0RETx, STM32G0B0VETx, STM32G0B1C(C-E)Tx, STM32G0B1C(C-E)Ux, STM32G0B1K(C-E)Tx, STM32G0B1K(C-E)TxN, STM32G0B1K(C-E)Ux, STM32G0B1K(C-E)UxN, STM32G0B1M(C-E)Tx, STM32G0B1R(C-E)Ix, STM32G0B1R(C-E)Tx, STM32G0B1V(C-E)Ix, STM32G0B1V(C-E)Tx, STM32G0C1C(C-E)Tx, STM32G0C1C(C-E)Ux, STM32G0C1K(C-E)Tx, STM32G0C1K(C-E)TxN, STM32G0C1K(C-E)Ux, STM32G0C1K(C-E)UxN, STM32G0C1M(C-E)Tx, STM32G0C1R(C-E)Ix, STM32G0C1R(C-E)Tx, STM32G0C1V(C-E)Ix, STM32G0C1V(C-E)Tx
• Added the support for two new STM32G0 boards: NUCLEO-G0B1RE and STM32G0C1E-EV
• Added the support for new part numbers in the STM32H7 Series: STM32H735VGHx, STM32H725V(E-G)Hx
• Added the support for new part numbers in the STM32L4 Series: STM32L451CETx, STM32L452CETx and STM32L462CETx
• Added the support for new part numbers in the STM32L0 Series: STM32L073CZYx.
• Added the support for the STM32WL Series:
– Added the support for new part numbers in the STM32WL Series: STM32WL54CCUx, STM32WL54JCIx, STM32WL55CCUx, STM32WL55JCIx, STM32WL55UCYx, STM32WLE4C(8-B-C)Ux, STM32WLE4J(8-B-C)Ix, STM32WLE5C(8-B-C)Ux, STM32WLE5J(8-B-C)Ix, STM32WLE5U(8-B)Yx
– Added the support for two boards: NUCLEO-WL55JC1 and NUCLEO-WL55JC2
– Possibility to create a single or dual-core project. For dual-core projects, possibility to assign peripherals to the Cortex®-M0+ or Cortex®-M4 core
• Added LL support for I2S peripheral for the STM32G0 Series, STM32G4 Series, STM32WB Series and STM32WL Series
• Added the support for new features in the STM32MP1 Series:
– USART Smartcard mode – UART RS-485 mode
– FMC PSRAM support
• Added the support for one new STM32MP1 board: STM32MP157F-DK2
• Added Zigbee® support for the STM32WB Series: Channel selection, Endpoint selection, Cluster selection and allocation, and Cluster callback management
• Added the possibility for users in Mainland China to access to the video tutorials at stmcu.com.cn
• Added some search enhancements for the video tutorials feature
• Added the support of software packs for the dual-core STM32H7 Series and for the Cortex®-M4 of the STM32WL Series
• Added some enhancements in Example selector feature.
• Added the support for one new STM32L4 board: NUCLEO-L4A6ZG
• New access to External Tools on STM32CubeMX home page
Main fixed issues V6.1.0
73285 [MX-MP] [USART] Missing modes.
74932 ADC on STM32G0 and STM32WL, must have restricted channel list and sequencer configured first.
84914 [MX-CodeGen] STM32CubeMX tpl_main_c.ftl (main.c template) does not trap Error_Handler.
89910 [MX-G0] [Pinout] Remove ADC1_IN11 from PB7.
90913 [MX-L4+] [LPUART] Wrong code generated
90919 [MX] [SAI] Synchronous Slave mode always grayed and not available.
91032 [MX-H7] [LWIP] Generation errors with ethernetif.c.
91276 [MX-WB] [RCC] WS grayed and stuck on 3.
91939 [MX-F1] [ADC3] Missed code related to regular conversion parameter.
92551 [MX-G4] [TIM] Code generation for TIMx encoder mode with remap issue.
92818 [MX-NVIC] All IRQ priorities must be set automatically
link:
2020-12-08 7:16 AM
I start from CubeMX and open the project using CubeIDE with CubeMX version 6.1 and CudeIDE 1.5 and still get pretty much incomplete Init of GPIO when I set all defaults on STM32H747-DISCO
https://community.st.com/s/question/0D53W00000NUOGLSA5/cubemx-gpio-not-initialized-in-stm32h747disco
2021-01-09 5:09 PM
Sorry, I did not explore fully the GPIO in CubeMX for dual core like the H747.
You may need to assign which core will need to init it.