cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE not generate code for GPIO pin

Entony
Associate II

We are using the STM32WL55CCU6 processor and generating code for two cores. For GPIO it is not possible to specify which core will initialize the GPIO (of course, it is not necessary) but the code and definitions are not generated for any core.

Entony_1-1741332753899.png

STM32CubeIDE Version: 1.18.0

ioc file included...

1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @Entony 

First let me thank you for posting.

Concerning the issue of  no Pin Context Assignement option for GPIO , a ticket has been raised to dev team to correct this behavior ( Internal ticket number 200353 )

Concerning the missing generated code for GPIO , a ticket has been raised to dev team for fix (Internal ticket number 204824)

 

THX

Ghofrane