2023-09-03 03:53 AM
Solved! Go to Solution.
2023-09-04 06:11 AM
Hope this works for you ☺️
2023-09-04 06:16 AM
I always installed with sudo. The directory is by default: "home/STM32Cube/repository/"
2023-09-04 06:20 AM
You can change the default repository when opening your CubeIDE.
2023-09-04 07:23 AM
Realese 1.12.1 works fine, 1.13.1 still doesn't work.
Can multiple releases coexist on the same computer?
2023-09-04 07:55 AM
Yes, you can have multiple release in the same computer
Best regards.
II
2023-09-04 09:39 AM - edited 2023-09-04 09:44 AM
Thank you very much.
Now I have 1.10.1 and 1.12.1, they work fine. 1.13.1 does't work
If you want I can post the logs of 1.13.1
2023-09-04 09:42 AM - edited 2023-09-04 05:25 PM
Ok thanks.
Best regards
II
2023-09-04 02:32 PM
I will continue my work with release 1.12.1 while waiting for the solution to the problem of release 1.13.1.
Thanks for your help.
2023-09-04 03:42 PM
> If your question is answered please check this answer as best answer to be diffused.
> If that works fine. Close this topic by marking this answer as best answer.
> If your question is answered please check the answer as best answer to be diffused.
Seriously? It seems that begging three times is not enough - try writing it in every post at the beginning and the end!
And the answers are not "diffused". Probably you mean "spread" or something like that. Actually the word "diffusion" is a pretty international word and is the same in almost all languages. It's somewhat strange to not know it's meaning...
2023-09-04 03:49 PM
Hello @Piranha
I'm a new community member. Thanks for your feedback and I will try to correct .
Best regards.
II