cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.6.0, STM32H7 1.9.0: CubeMX sets I2S_InitTypeDef::Mode to I2S_MODE_SLAVE_TX instead of I2S_MODE_SLAVE_FULLDUPLEX

KBass.1
Associate
3 REPLIES 3
Khouloud ZEMMELI
ST Employee

Hello @KBass.1​ 

Thanks for your feedback, could you please share your ioc file to check the config and the part number used?

Khouloud

KBass.1
Associate

I can't access the .ioc file right now, but I'm using a NUCLEO-H743ZI2​ and the issue happens when setting I2S3 to Full-Duplex Slave mode.

Hi @KBass.1​ 

Thank you for specifying the part number used which helped me to reproduce the issue, it's linked to some PN and not to all H7 serie.

In fact, this problem is due to the presence of the Transmission mode parameter in the configuration part, so that the mode value will be taken directly from there.

Issue will be fixed, thanks again for raising such a problem to our attention and for your contribution.

Khouloud