2024-12-01 02:43 AM
Hi All
I have installed STM32 CubeMX on a Mac and I get the following error when trying to generate code:
The Eclipse executable launcher was unable to locate its companion shared library.
2024-12-02 12:24 AM
2024-12-02 09:14 PM
I encountered exactly the same issue. I’m trying to compile STM32 projects on a Mac using CubeMX and CLion, but every time I click “Generate Code” in CubeMX, it throws this error, causing CLion to fail to compile. It shows the message: “No project sources generated. Run Generate Code in CubeMX.” MacBook Air M1.
2024-12-03 09:40 AM
I use 15.1.1
2024-12-03 09:43 AM
When I rolled the CubeMX version back to 6.12, I didn't have this problem. This problem appeared when the CubeMX version was 6.13.
2024-12-04 01:20 AM
Have you selected STM32CubeIDE to generate your project? If yes, what version of CubeIDE do you have?
2024-12-04 01:50 AM
I also encountered the same problem as you, but the problem still exists after I returned to version 6.12
2024-12-04 02:27 AM
I selected STM32CubeIDE to generate your project, and I use Clion as my IDE
2024-12-04 04:57 AM
2024-12-04 04:59 AM
My cubeide and cubemx are both the latest versions. When cubemx selects cubeide in the toolchain, it will display Eclipse related reminders