cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 CubeMX - Generate Code fails on a Mac (Apple Silicon)

fabltd
Associate III

Hi All

I have installed STM32 CubeMX on a Mac (Apple Silicon) and I get the following error when trying to generate code:

The Eclipse executable launcher was unable to locate its

companion shared library.

Any one come accross this and any idea how to fix?

 

9 REPLIES 9
mƎALLEm
ST Employee

Approximately the same issue as :https://community.st.com/t5/stm32cubemx-mcus/cubemx-fails-to-generate-project-on-apple-silicon/td-p/728310

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi 

No solution offered. The reply askes for a windows path?

The reply askes for a windows path?

Not quite. Just provide any relevant log that you have on your Mac.

By the way, the Windows path. A Windows PC with trusted and powerful x64 platform provides best experience for Cube* tools. You just stay productive and hassle free most of the time.

 

Hi

This is a windows path C:\Users\XXXXX\STM32CubeIDE\workspace_1.16.1\.metadata? 

No C: on a mac.

The mac path is simular and the contents of the file are:

Fri Oct 25 16:43:22 BST 2024

org.eclipse.core.runtime=2

org.eclipse.platform=4.30.0.v20231201-0110

 

Deleting the metadata file also makes no difference to the error.

Should the be a seperate file for MX the path was for the IDE

".metadata" is a directory. In this directory, look for files ".log"  and ".ide.log"

 

fabltd
Associate III

I can see the files but what am I looking for?

fabltd
Associate III

When I remove .log and .ide.log they are not recreated by STM32 Cube MX. 

This directory only gets updated by the IDE and not STM32 Cube MX from what I can see?

fabltd
Associate III

Screenshot 2024-10-25 at 18.34.12.png

 

If I change the tool chain from STM32CubeIDE to for example EWARM the error is not present.