2014-08-23 1:14 AM
Does somebody know when the F1 devices will be completely supported on STM32 Cube(i.e. STM32F103)?
#stmcube-stmcubemx #stm32f12014-09-05 7:17 AM
Hi pejic.predrag.001,
The STM32CubeF1 release target is very end of year.Thank you for your interest in our STM32Cube solution.With regards.2014-12-01 4:07 AM
Hello Heisenberg,
are there any news about the release date for full support of F1 devices in CubeMX? I.E: STM32F103ZG? Thank you! Regards Bernhard2014-12-07 4:51 AM
Hi. I also very wait for F1 support. Maybe some BETA version is available.
2014-12-08 4:35 AM
Hi,
any new updates about F1 release?2014-12-17 9:32 AM
I also would like to know if there is any updates on the release.
I don't want to go learning to use the older std. library since when i start to work (still studying) the stm32cube will be more mature (and looks promissing so far).2015-01-05 10:42 PM
Any update on Cube for F1 family ?
waiting...2015-01-15 6:21 AM
Here too, I have some software that I use on both F103 and F401 parts.
It was bad enough having two separate libraries with subtly different names, but now I've got the STM32 cube libs for the F401 part and the old libraries for the F103, suddenly all the function names for one device are pointlessly prefixed with 'HAL_' and on the other device they're not. It makes sharing code pretty much impossible.