2015-07-06 9:20 AM
Hi to all, i'm a newbie of programming embedded, i have a Stm nucleo L152RE and i a sd card shiled v 4.1 of seeed studio this is the
of shiled. Now i want use cubemx for use this shield, i use this setting: PERIPHERALS MODES FUNCTIONS PINS RCC Crystal/Ceramic Resonator RCC_OSC_IN PH0-OSC_IN RCC Crystal/Ceramic Resonator RCC_OSC_OUT PH1-OSC_OUT SPI1 Full-Duplex Master SPI1_MISO PA6 SPI1 Full-Duplex Master SPI1_MOSI PA7 SPI1 Full-Duplex Master SPI1_SCK PA5 SYS Trace-Asynchronous_SW SYS_JTMS-SWDIO PA13 SYS Trace-Asynchronous_SW SYS_JTCK-SWCLK PA14 SYS Trace-Asynchronous_SW SYS_JTDO-TRACESWO PB3 USART2 Asynchronous USART2_RX PA3 USART2 Asynchronous USART2_TX PA2 Pin Nb PINs FUNCTIONs LABELs 2 PC13-WKUP2 GPIO_Input B1 [Blue PushButton] 3 PC14-OSC32_IN* RCC_OSC32_IN 4 PC15-OSC32_OUT* RCC_OSC32_OUT 5 PH0-OSC_IN RCC_OSC_IN 6 PH1-OSC_OUT RCC_OSC_OUT 16 PA2 USART2_TX USART_TX 17 PA3 USART2_RX USART_RX 21 PA5 SPI1_SCK 22 PA6 SPI1_MISO 23 PA7 SPI1_MOSI 46 PA13 SYS_JTMS-SWDIO TMS 49 PA14 SYS_JTCK-SWCLK TCK 55 PB3 SYS_JTDO-TRACESWO SWO 57 PB5 GPIO_Output I select FatFs to read and write on SDcard now i generete the code i don't see the file sd_diskio.c, can you give me example or how to, for setting and use it. best regards Antonio #cubemx #nucleo #spi2015-07-07 8:37 AM
2015-07-09 8:33 AM
What Antonio said is that cubeMX don't generate all the necessary files. This bug has been discovered several times :
- [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Is%20stm32cubemx%20v4.8%20a%20beta&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=106]bug 1- [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/cubemx%20v4.8%20-%20fatfs&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx¤tviews=40]bug 2I can reproduce it with v4.8, STM32F4, new project from scratch. In other words,- We are not able to update our existing projects with cubemx- We are not able to create new projects with cubemx- People that are not familiar with STM32 will switch to other equivalent processors- People that are familiar with STM32 will certainly switch to other equivalent processors in a few months, after they loosed a lot of money, is ST don't fix the bug.- Expressed as a simple manner for ST (in case they don't understand), *ST will loose money* (and there are already in a very poor economical state here in France).Workaround for any people that don't want to wait: SD cards / fatfs works fine without effort on SAM processors.2015-07-09 11:19 AM
Hi Antonio,
Without knowing more about the configuration, quite hard to reproduce (in fact, not reproduced yet, works fine for me with Mx 4.8, IAR, Win OS7: files always generated).
Would it be possible to know:
- CubeMx version in use: 4.x (with x = ?) ; standalone executable installed or Eclipse plugin used? - OS : Linux / Windows 7, 8 or 10 ? - toolchain being used : IAR / Keil / Atollic / SW4STM32 / ... ? Getting your project file (the one with .ioc extension) could help as well (unless it contains confidential data)Something I have already said in a recent FreeRTOS discussion: we need to know tools and OS versions you use for a better support.
Regards,
Fred
What Antonio said is that cubeMX don't generate all the necessary files. This bug has been discovered several times :
- [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Is%20stm32cubemx%20v4.8%20a%20beta&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21¤tviews=106]bug 1 - [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/cubemx%20v4.8%20-%20fatfs&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx¤tviews=40]bug 2 I can reproduce it with v4.8, STM32F4, new project from scratch. In other words, - We are not able to update our existing projects with cubemx - We are not able to create new projects with cubemx - People that are not familiar with STM32 will switch to other equivalent processors - People that are familiar with STM32 will certainly switch to other equivalent processors in a few months, after they loosed a lot of money, is ST don't fix the bug. - Expressed as a simple manner for ST (in case they don't understand), *ST will loose money* (and there are already in a very poor economical state here in France). Workaround for any people that don't want to wait: SD cards / fatfs works fine without effort on SAM processors.2015-07-10 5:25 AM
2015-07-14 12:58 AM
hi to all, thanks for your help
CubeMx version in use: 4.8.0; standalone O.S. windows 7 64 bit toolchain being used : Keil i am a newbie in embedded world and i am studying for understand to use it. can you see a easy example for learn it? best regards A. p.s. in Attachments you can see my ioc file. ________________ Attachments : sd_card4.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzTO&d=%2Fa%2F0X0000000bMK%2F2sEkVwXR5.Jy_Ppi1tUj4e2ZbODcL47Cg4q.3z.y97U&asPdf=false2015-07-17 7:09 AM
Hello Antonio,
The file you are looking for is under : Middlewares\Third_Party\FatFs\src\drivers. Depending on your choice of project settings to copy or to reference the library files, this directory may be copied under your project at project generation or only kept as reference to your cube repository (see in C:/users/<your username>/STM32Cube/Repository). Best regards.