cancel
Showing results for 
Search instead for 
Did you mean: 

STCUBEMX incomplete ThreadX code generation error on linux

sai2
Associate II

Hi,

When I tried to generate a project with ThreadX for STM32N6, STCUBEMX generated incomplete code.

CubeMX Ver : 6.14.0

MCU: STM32N6

Platform: Ubuntu 24.04

ioc file attached.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @sai2 ,

 

Thank you for bringing this issue to our attention.

An internal ticket is raised to the Development team under this number: 207773.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Mahmoud Ben Romdhane
ST Employee

Hello @sai2 ,

 

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

I suggest also that you provide a capture of the issue.

 

Best Regards.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I attached a build log and screenshot of the folder structure. As you can see in the screenshot, there are duplicated cortex_m55 and cortex_M55 folder generated under middleware/ST/threadx/ports and there are no source code generated under middleware/ST/threadx/ports/cortex_M55/gnu/src. Generating project under window environment works and dont have duplicated "cortex_M55" folder.

There is another issue surfaced when I tried to import example application, which also result in incompleted project and was unable to build. Again, importing example project under window environment works fine.

Steps to reproduce:

1. Import STM32Cube Example

2. select "Ux_Host_VIDEO" example for "STM32N6570-DK"

3. build (fail)

error (for some reason I was unable to post the log file for example project)

make: *** No rule to make target '/home/sai/STM32CubeIDE/workspace_1.16.1/Ux_Host_VIDEO/Middlewares/ST/threadx/ports/cortex_m55/gnu/src/tx_misra.s', needed by 'Middlewares/ThreadX/Port/tx_misra.o'. Stop. make: *** Waiting for unfinished jobs.... "make -j14 all" terminated with exit code 2. Build might be incomplete.

 

Hello @sai2 ,

 

Thank you for bringing this issue to our attention.

An internal ticket is raised to the Development team under this number: 207773.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I'm also facing this issue with STM32CubeMX 6.14.1, also working with the N6, on Linux. Do you recommend any workaround?