2024-11-01 8:03 AM
EMB1428QSQ/NOPB is used which has the frequency of the 1.1MHz fclk and the SPI2 of STM32F469BIT7 is going as a clock to it. I need the minimum value of the SPI2 master that can be fed to the EMB1428QSQ/NOPB. Also, where can I find the minimum frequency of the communication interfaces , I have used the USART and SPI2.
Solved! Go to Solution.
2024-11-01 8:07 AM - edited 2024-11-01 8:07 AM
Hello,
Why are you looking for the minimum freq value?
Only maximum values are provided in the datasheet:
And you can go downto 1MHz for SPI
2024-11-01 8:07 AM - edited 2024-11-01 8:07 AM
Hello,
Why are you looking for the minimum freq value?
Only maximum values are provided in the datasheet:
And you can go downto 1MHz for SPI
2024-11-01 8:08 AM - edited 2024-11-01 8:09 AM
@deeksha23jan wrote:EMB1428QSQ/NOPB .
You mean this: https://www.ti.com/product/EMB1428Q/part-details/EMB1428QSQ/NOPB ?
@deeksha23jan wrote:I need the minimum value of the SPI2 master that can be fed to the EMB1428QSQ/NOPB.
Also, where can I find the minimum frequency of the communication interfaces
The minimum required by the EMB1428QSQ will be specified in the EMB1428QSQ datasheet;
The minimum that can be provided from the STM32 will be specified in the STM32 datasheet and/or Reference Manual:
https://www.st.com/en/microcontrollers-microprocessors/stm32f469bi.html#documentation