Simple I2S app on STM32G0136-disco is failing
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-27 8:43 AM
I have created a simple app using stm32cubemx and cubeide that waits for a GPIO signal to go low, then plays a canned stream of I2S data to the port. The function call to HAL_I2S_Transmit() is causing the system to reset. Specifically the statement: __HAL_I2S_ENABLE(hi2s) causes the i2C output signals to transition into the active state, then the chip resets.
I've generated the init code with MX and get no compile errors or warnings. I've attached the project.
Thanks,
Scott
- Labels:
-
I2S
-
STM32CubeMX
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-28 10:51 PM
> Specifically the statement: __HAL_I2S_ENABLE(hi2s) causes the i2C output signals to transition into the active state
It's unlikely - that macro probably just sets I2SE in SPIx_I2SCFGR.
Single-step the code in disasm - does write to SPIx_I2SCFGR indeed cause I2C signals to go down?
Try to divide and rule - disable interrupts from I2S and see what happens.
I also assume there's nothing more in the code than I2C and I2S - if yes, remove it to achieve the bare minimum exhibiting the problem.
JW
PS. Please change your user name to a normal nick.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-29 4:25 AM
Hi Jan,
Thanks for the reply. Yes, this code is running on the stm32g0136-disco board. But isn't MX supposed to generate workable code? Is there an interrupt assignment I am missing, even though I am using the polled calls?
Thanks,
Scott
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-02 9:44 AM
I thought perhaps there was an uninitialized interrupt vector, so I added __disable_irq() to my code after initialization. It didn't make any difference.
Even though "It's unlikely - that macro probably just sets I2SE in SPIx_I2SCFGR", single step tracing through that statement shows the reset handler with the IP set to mov sp,r0.
.section .text.Reset_Handler
.weak Reset_Handler
.type Reset_Handler, %function
Reset_Handler:
ldr r0, =_estack
mov sp, r0 /* set stack pointer */
/* Copy the data segment initializers from flash to SRAM */
movs r1, #0
b LoopCopyDataInit
CopyDataInit:
ldr r3, =_sidata
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4
LoopCopyDataInit:
ldr r0, =_sdata
ldr r3, =_edata
adds r2, r0, r1
cmp r2, r3
bcc CopyDataInit
ldr r2, =_sbss
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-02 12:23 PM
So, it goes into reset? Is anything external connected, or is this only the "pure" DISCO board? Can't the shared pins be in conflict with each other? How exactly are the relevant GPIO registers set just before that macro, as read out by the debugger?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-02 1:01 PM
Hi Jan,
It is a disco board that I have wired to an Atmel D21 Xplained Pro (as a source of I2C data) and a MAX98357A a speaker driver. I have the MX project configured only as a I2S master using pins 4, 5 & 6 and pins 7 & 8 for the debugger. Pin 1 is a GPIO input, so I don't think the reset function is enabled. I will check over the settings for the reset controller to see if it is enabled in spite of not being named as a reset input.
Thanks,
Scott
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-02 2:29 PM
Scott,
I mean, two connected pins, bith turned to output with different polarities. That might have caused a reset through a power supply drop.
Disconnect the external device and try again.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-03 6:46 AM
Hi Jan,
With all pins disconnected, the CPU still resets at the __HAL_I2S_ENABLE(hi2s) macro.
Scott
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-03 7:41 AM
The 8-pin package has several pins connected internally. Maybe these are in conflict.
How exactly are the GPIO registers set just before that macro, as read out by the debugger?
Read them out and check/post.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-11-03 1:27 PM
Hi Jan,
Here are the GPIO register values. All values not listed are zero. This is in hex integer format, so 0x80000000 is bit 31 set.
50000000 EAFFFFFB 00000000 0C000000 24000000
50000010 00004002 00000000 00000000 00000000
50000400 FFFFFFFE 00000000 00000000 00000000
50000800 CC00F000 00000000 00000000 00000000
50000C00 000000FF 00000000 00000000 00000000
Thanks,
Scott