2018-11-01 07:01 PM
CubeMX generated code to enable RTC Wakeup starts with HAL_RTC_Init but the examples in the HAL library 'unlock' the RTC via the PWR module using HAL_PWR_EnableBkUpAccess.
Which is correct? CubeMX or Example code in HAL?
2018-11-02 07:08 AM
Hello @frackers ,
We will check this issue, then we come back to you as soon as possible.
Kind Regards,
Imen.