2023-07-15 02:58 PM
The new version of CubeMX (6.9.0) no mater of options in Project Manager / Code Generator, if Keil Toolchain / IDE is choosen, the project regeneration delete the previous .uvprojx file and generates a new one, LOOSING ALL changes made by the user in the project. For now, I uninstalled the new version and went back to the previous one (6.8.1). Any solutions I haven't seen?
Meanwhile, I continue with the aforementioned problem (CubeMX messed up) and there is no way to solve it (I'm honestly disappointed...)
2023-07-17 06:07 AM - edited 2023-07-17 06:29 AM
Hello @Luiz Pereira
Thank you for having reported.
I assume this is the exact same issue already reported to the development team and tracked by the Ticket 157222 and that will be fixed as soon as possible.
The issue is detected only when you use keil Toolchain , in the other hand STM32CubeIDE 1.13.0 and EWARM work correctly : they do not delete the added user file after regeneration.
Thx
Ghofrane
2023-07-17 05:05 PM
Thanks for the update. It is effectievlly the issue reported. I will wait for news.
BTW, is there any explanation for the problem (and I saw that it has also been reported but without solution) with CubeMX's UI interface?
Thanks again
Luiz
2023-07-18 05:47 AM
can confirm this. should have checked here before updating.
everytime after i update cubemx or touchgfx different things are broken