cancel
Showing results for 
Search instead for 
Did you mean: 

Selecting HSE as clock gives error

User2501
Associate II

Hello, 

I have a problem trying to create a project in STM32CubeMX with a custom board using STM32L476RGT6 with crystal oscillator of 32MHz. In the interface configuration, when I selected HSE and set the value of 32MHz, it failed to initialize the peripherals because it got caught in a loop error by the clock configuration of the system. I have also verified the crystal signal and it corresponds to the frequency and if i select other options like HSI, everything works fine.

Looking for your advice to solve this problem, 

Best regards, 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @User2501 

First, I want to thank you for posting.

I tried the STM32 project which you described using the STM32CubeMX 6.9.1 version and I had 0 warnings and 0 errors.

I advise you to reproduce your project with the last version and I will be waiting for your feedback.

Thx.

Mahmoud.

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

waclawek.jan
Super User

> it got caught in a loop error by the clock configuration of the system

What does that exactly mean? What loop? What causes it? Single-step through the clock setup routine to find out - Cube is open source so you can do that.

> crystal oscillator of 32MHz

Is it a *crystal* or a *crystal oscillator*? Which model? If the latter, do you set RCC_CR.HSEBYP?

JW

TDK
Super User

Perhaps there's an issue with your hardware. Perhaps incorrect values on load capacitors. Can you share the schematic?

If you feel a post has answered your question, please click "Accept as Solution".