cancel
Showing results for 
Search instead for 
Did you mean: 

RTC wakeup with CubeMX generated code does not work.

SAkhi.951
Associate III

I have setup RTC wakeup functionality and generated code with CubeMX.

The code does not work straight away, because imr1's mr20 in EXTI IMR1 register was not unmasked. I suppose this is a bug and should be handle by STM. It took some time to figure that out and that is not what you expect from automatic code generator.

Note! This is just a bug report and notice for everyone who faced same issue.

/* RTC init function */
void MX_RTC_Init(void)
{
 
  /** Initialize RTC Only
  */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
  hrtc.Init.AsynchPrediv = 127;
  hrtc.Init.SynchPrediv = 255;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    Error_Handler();
  }
  
  if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 7, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
  {
    Error_Handler();
  }
  
 /* Adding this line makes Wake up ISR works */
  __HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_IT(); 
}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Khouloud ZEMMELI
ST Employee

Hello @SAkhi.951​ 

Thanks for your feedback,

Which part number are you using please?

Khouloud

Hello @Khouloud ZEMMELI​ ,

MCU - STM32L41RCIx. CubeMX FW package FW_L4 V1.13.0